IMX8mm SPI issue with XR20M1172 spi to dual uart

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8mm SPI issue with XR20M1172 spi to dual uart

5,661件の閲覧回数
Himanishu
Contributor I

I am using IMX8MM processor and connecting SPI to dual UART XR20M1172 over spi2 but I am getting error.

Device tree entry :

xr20m1172: xr20m1172@0 {
            compatible = "exar,xr20m1172";
            reg = <0>;
            clock-frequency = <14745600>;
            interrupt-parent = <&gpio>;
            interrupts = <&gpio 6 IRQ_TYPE_EDGE_FALLING>;
            gpio-controller;
        };
 

 

Getting below logs from console 

root@lec-imx8mm:~# dmesg | grep spi
[ 2.856874] spi_drv_probe+0x4c/0xe4
[ 2.925573] spi_add_device+0xf4/0x1f0
[ 2.929322] of_register_spi_device+0x20c/0x39c
[ 2.933853] spi_register_controller+0x5f0/0x8d0
[ 2.938471] spi_bitbang_start+0x4c/0x80
[ 2.942396] spi_imx_probe+0x420/0x6a0

I have attached the complete dmesg file for reference 

 

0 件の賞賛
返信
4 返答(返信)

5,633件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what error do you get? could you get any signal from your device? and pls tell me your bsp version and send to me your entire dts file

0 件の賞賛
返信

5,622件の閲覧回数
Himanishu
Contributor I

Linux kernel version 5.10.72

I have attached the XR20M1172 driver file, device tree file and dmesg file for reference.

on chip select pin continuous 3.3 voltage observing and no node created in /dev/

 

0 件の賞賛
返信

5,481件の閲覧回数
Himanishu
Contributor I

@joanxie Did you get a chance to see the above details 

0 件の賞賛
返信

5,461件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

refer to the logfile, I don't find any error message about SPI

0 件の賞賛
返信