How to know the irq number for the UART3 module on i.MX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to know the irq number for the UART3 module on i.MX6Q

Jump to solution
2,390 Views
yinliangren
Contributor II

   I'd like to set IRQ to CPU1 on i.MX6Q sabresd board like : 

                                   echo 2 > /proc/irq/irqnumber/smp_affinity

 But I didn't find the irq number for UART3 module, could somebody help me? 

BTW, the BSP version is 5.10.72_2.2.0.

0 Kudos
Reply
1 Solution
2,323 Views
yinliangren
Contributor II

I've got the number, it's not a constant number. The irq number showed up after I ran an application to open and use UART3. 

View solution in original post

3 Replies
2,374 Views
Yuri
NXP Employee
NXP Employee

@yinliangren 
Hello,

   According to Table 3-1 (Arm Cortex A9 domain interrupt summary) of i.MX 6Dual/6Quad Reference Manual (Rev. 6, 05/2020) IRQ = 60 for  UART3 interrupt request.

Regards,
Yuri.

0 Kudos
Reply
2,366 Views
yinliangren
Contributor II

Hi Yuri,

   Thanks for your answer, but I haven't found the number 60 in /proc/irq/ as below:

root@imx6qsabresd:~# uname -a
Linux imx6qsabresd 5.10.72-lts-5.10.y+ga68e31b63f86 #1 SMP PREEMPT Tue Nov 23 06:02:20 UTC 2021 armv7l armv7l armv7l GNU/Linux
root@imx6qsabresd:~#
root@imx6qsabresd:~# ls /proc/irq/
100/ 291/ 72/
118/ 30/ 73/
123/ 31/ 74/
125/ 315/ 77/
147/ 32/ 78/
16/ 33/ 79/
17/ 34/ 80/
171/ 35/ 81/
178/ 51/ 82/
18/ 52/ 83/
181/ 57/ 84/
184/ 58/ 85/
19/ 62/ 86/
20/ 63/ 87/
21/ 64/ 88/
22/ 65/ 89/
221/ 66/ 90/
23/ 67/ 95/
24/ 68/ 96/
25/ 69/ default_smp_affinity
26/ 70/
28/ 71/

Could you tell me how to show 60 in /proc/irq/ ? Thanks a lot.

Tags (1)
0 Kudos
Reply
2,324 Views
yinliangren
Contributor II

I've got the number, it's not a constant number. The irq number showed up after I ran an application to open and use UART3.