How to configure an external crystal for KL05 in Processor Expert Software?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to configure an external crystal for KL05 in Processor Expert Software?

1,779件の閲覧回数
thoomanwang
Contributor V

I tried Processor Expert Software Software for KL06Z16 configure an external crystal , but I tried all the usual crystal , are unable to set the system frequency to 48MHz.
Am I doing something wrong is it ?

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,053件の閲覧回数
thoomanwang
Contributor V

This issue has been resolved , the KL04, 05 can only use the internal oscillator or an external 32.768KHz crystal oscillator frequency can configure the system to 48MHz, other crystals are not available .

0 件の賞賛
返信

1,053件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi,

Yes, you can use 32 kHz but generally, you can use  any crystal up to 32 MHz in a bypass mode or with FLL engaged.

If you want to get 48MHz core clock you can also use 9.6MHz crystal (the FLL clock generator has only few options of multiplication so the number of possible clock values is quite limited).

You can set it up in the Processor Expert CPU component using the inspector the following way:

KL05ExtCrystal.png

best regards

Petr Hradsky

Processor Expert Support Team

0 件の賞賛
返信