I am running CW 10.5 Build 130916
I have generated SPI code for the K60DN512VMD10 chip (for SPI2)
In the attribute set list section, it will only accept 1 and 16 for both the HW input buffer size and the HW output buffer size.
This is incorrect (AFAICT), the values should be 1 or 4.
However, I am not sure this affects any of the generated code at all.
How important is this error?