How important is it that the PE FIFO size for K60 SPI peripherals is wrong?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How important is it that the PE FIFO size for K60 SPI peripherals is wrong?

Jump to solution
1,516 Views
Symbolic
Contributor III

I am running CW 10.5 Build 130916

I have generated SPI code for the K60DN512VMD10 chip (for SPI2)

In the attribute set list section, it will only accept 1 and 16 for both the HW input buffer size and the HW output buffer size.

This is incorrect (AFAICT), the values should be 1 or 4.

However, I am not sure this affects any of the generated code at all.

How important is this error?

Tags (3)
0 Kudos
Reply
1 Solution
1,281 Views
vfilip
NXP Employee
NXP Employee

Hello,

I must confirm that this is really bug in latest version of PEx. However I think it should not influence code functionality. You can for example compare generated code when you set buffer size to 1 and to 16, the only difference is in DIS_TXF/DIS_RXF bitfields in MCR register. DIS_TXF/DIS_RXF bit-fields disable/enable FIFO -> size 4 or 16 should not influence driver functionality.

We will fix it for next release of PEx.

We are sorry for inconvenience.

Best regards

Vojtech Filip

Processor Expert Support Team

View solution in original post

0 Kudos
Reply
1 Reply
1,282 Views
vfilip
NXP Employee
NXP Employee

Hello,

I must confirm that this is really bug in latest version of PEx. However I think it should not influence code functionality. You can for example compare generated code when you set buffer size to 1 and to 16, the only difference is in DIS_TXF/DIS_RXF bitfields in MCR register. DIS_TXF/DIS_RXF bit-fields disable/enable FIFO -> size 4 or 16 should not influence driver functionality.

We will fix it for next release of PEx.

We are sorry for inconvenience.

Best regards

Vojtech Filip

Processor Expert Support Team

0 Kudos
Reply