Hi:) I would like to ask about the use of PWM_Ldd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi:) I would like to ask about the use of PWM_Ldd

912件の閲覧回数
priscillayeung
Contributor I

Hi :smileyhappy:

If I want to control the speed of changing LED colours using different position of the touch slider, can I add another pwm ldd to the same led?

Thanks :smileyhappy:

ラベル(1)
0 件の賞賛
返信
1 返信

695件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

I do not find necessary adding another pwm component to the LED, you can vary the frequency of the PWM and the duty cycle with the same PWM_LDD component.

You may find useful these post by colleague Erich Styger:

Tutorial: Touching the Freedom KL25Z Board | MCU on Eclipse

Tutorial: PWM with Processor Expert | MCU on Eclipse


Hope this information can help you.

Best Regards,
Adrian

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信