Hi
I am using CodeWarrior 10.6 and Processor Expert to generate Ethernet LDD. The code supplied runs on TWR-K60N512 and in just a few seconds reproduce my problem.
Problem is that I get one more OnFrameTransmitted than actual SendFrame's. When this occurrs it is always when OnFrameTransmitted interrupts an ongoing SendFrame. From a user perspective it is easy to say that I don't want more completed frame receipts than what I have scheduled for sending, but finding logical explanation to it is harder.
Please have a try on attached project and se for yourself! More info in main.c on steps to reproduce problem.
Regards
/Peter
Original Attachment has been moved to: EthernetPE.zip
已解决! 转到解答。
Hi
After investigation of this problem, I think I found the root cause of problem.
SendFrame adds to TxQueue in two steps. First without TX_READY flag and then in next step TX_READY flag is added.
The TX_READY flag is reset when ethernet peripheral has sent it.
InterruptTxFrame checks that TX_READY is reset to determine if OnFrameTransmit should take place.
Now, when interrupt occurrs between step 1 and 2 of SendFrame above, the frame is wrongly interpreted as already sent since the bit TX_READY is not yet set.
One solution is:
1) Add another flag, ETH1_TX_TO1, or-ed to TX_READY in step 2.
LDD_QUEUE_GET_TAIL_OFFSET_ITEM(DeviceDataPrv->TxQueue, BufferDescCount - Index).Flags |= ETH1_TX_READY; /* Enable buffer transmission */ |
LDD_QUEUE_GET_TAIL_OFFSET_ITEM(DeviceDataPrv->TxQueue, BufferDescCount - Index).Flags |= |
ETH1_TX_READY | /* Enable buffer transmission */ |
ETH1_TX_TO1; /* Indicate that it has been enabled */ |
2) Add check for TX_TO1 in RemoveTxFrame
!(LDD_QUEUE_GET_HEAD_OFFSET_ITEM(DeviceDataPrv->TxQueue, BufferOffset).Flags & ETH1_TX_READY)) { |
!(LDD_QUEUE_GET_HEAD_OFFSET_ITEM(DeviceDataPrv->TxQueue, BufferOffset).Flags & ETH1_TX_READY) && |
(LDD_QUEUE_GET_HEAD_OFFSET_ITEM(DeviceDataPrv->TxQueue, BufferOffset).Flags & ETH1_TX_TO1)) { |
Hope this helps!
Regards
/Peter
Hi
After investigation of this problem, I think I found the root cause of problem.
SendFrame adds to TxQueue in two steps. First without TX_READY flag and then in next step TX_READY flag is added.
The TX_READY flag is reset when ethernet peripheral has sent it.
InterruptTxFrame checks that TX_READY is reset to determine if OnFrameTransmit should take place.
Now, when interrupt occurrs between step 1 and 2 of SendFrame above, the frame is wrongly interpreted as already sent since the bit TX_READY is not yet set.
One solution is:
1) Add another flag, ETH1_TX_TO1, or-ed to TX_READY in step 2.
LDD_QUEUE_GET_TAIL_OFFSET_ITEM(DeviceDataPrv->TxQueue, BufferDescCount - Index).Flags |= ETH1_TX_READY; /* Enable buffer transmission */ |
LDD_QUEUE_GET_TAIL_OFFSET_ITEM(DeviceDataPrv->TxQueue, BufferDescCount - Index).Flags |= |
ETH1_TX_READY | /* Enable buffer transmission */ |
ETH1_TX_TO1; /* Indicate that it has been enabled */ |
2) Add check for TX_TO1 in RemoveTxFrame
!(LDD_QUEUE_GET_HEAD_OFFSET_ITEM(DeviceDataPrv->TxQueue, BufferOffset).Flags & ETH1_TX_READY)) { |
!(LDD_QUEUE_GET_HEAD_OFFSET_ITEM(DeviceDataPrv->TxQueue, BufferOffset).Flags & ETH1_TX_READY) && |
(LDD_QUEUE_GET_HEAD_OFFSET_ITEM(DeviceDataPrv->TxQueue, BufferOffset).Flags & ETH1_TX_TO1)) { |
Hope this helps!
Regards
/Peter