Easy Importing of K60 pin assignments in Component Inspector?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Easy Importing of K60 pin assignments in Component Inspector?

跳至解决方案
1,393 次查看
rc
Contributor I

I'm new to using CodeWarrior PE and am trying to configure my K60 pin/resource assignments using the component inspector. Is there an easier way to assign pin names and resources, or does each pin have to be added manually? I'm thinking there is perhaps a way to import a text or pin file similar to an FPGA?

I haven't found much on this topic in the forums or CW help files but I'm thinking there must be an easier way than assigning each of these resources (and changing them when needed) individually?

Thanks

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,270 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

Yes, that would be a useful thing (to apply settings to a component in the project). As of MCU10.2, this is not supported yet.

But you can at least copy existing settings/components which might be helpful for you too:

http://mcuoneclipse.wordpress.com/2012/05/04/copy-my-component-settings-processor-expert-templates/

 

Hope this helps,

BK

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,271 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

Yes, that would be a useful thing (to apply settings to a component in the project). As of MCU10.2, this is not supported yet.

But you can at least copy existing settings/components which might be helpful for you too:

http://mcuoneclipse.wordpress.com/2012/05/04/copy-my-component-settings-processor-expert-templates/

 

Hope this helps,

BK

0 项奖励
回复