Easy Importing of K60 pin assignments in Component Inspector?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Easy Importing of K60 pin assignments in Component Inspector?

ソリューションへジャンプ
1,508件の閲覧回数
rc
Contributor I

I'm new to using CodeWarrior PE and am trying to configure my K60 pin/resource assignments using the component inspector. Is there an easier way to assign pin names and resources, or does each pin have to be added manually? I'm thinking there is perhaps a way to import a text or pin file similar to an FPGA?

I haven't found much on this topic in the forums or CW help files but I'm thinking there must be an easier way than assigning each of these resources (and changing them when needed) individually?

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,385件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

Yes, that would be a useful thing (to apply settings to a component in the project). As of MCU10.2, this is not supported yet.

But you can at least copy existing settings/components which might be helpful for you too:

http://mcuoneclipse.wordpress.com/2012/05/04/copy-my-component-settings-processor-expert-templates/

 

Hope this helps,

BK

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,386件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

Yes, that would be a useful thing (to apply settings to a component in the project). As of MCU10.2, this is not supported yet.

But you can at least copy existing settings/components which might be helpful for you too:

http://mcuoneclipse.wordpress.com/2012/05/04/copy-my-component-settings-processor-expert-templates/

 

Hope this helps,

BK

0 件の賞賛
返信