Does the new PE (v10.4) component inspector lost its ability to see the details in the assigned pins?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the new PE (v10.4) component inspector lost its ability to see the details in the assigned pins?

ソリューションへジャンプ
1,977件の閲覧回数
cesarrabak
Contributor III

In the PE 10.4 (which I have access to via KDS 1.1.1) I cannot find a means of seeing the "details" in the Resources view of the CPU component:

KDS-PEx-Resources.png

In the v10.3 (available in CW 10.6) I can see these details in a third column as can be seen in the figure below:

CW-10.6-PEx-Resources.png

Is this a change in the design and this information is now presented in another place?

Regards,

--

Cesar Rabak

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,355件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Cesar:

It seems that the new Tabs view is missing those details. But you can disable the Tabs_view and go back to classic, like this:

Tabs_view.png


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,356件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Cesar:

It seems that the new Tabs view is missing those details. But you can disable the Tabs_view and go back to classic, like this:

Tabs_view.png


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,355件の閲覧回数
cesarrabak
Contributor III

Hi Jorge Gonzalez!

Yep! There it is!

Thank you very much!

Now if I could find where is the Correct Answer button :smileyconfused:.  Maybe because I see the interface in a non English locale this doesn't appear?

x2scrap.png

0 件の賞賛
返信
1,355件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hi Cesar:

I'm glad it helped :smileyhappy:.

That is your inbox. Inbox only shows an overview of the thread, but to access the complete thread you have to click on the thread title. Then you can see the "Correct Answer" and "Helpful Answer" buttons (or in your case "Respuesta Correcta" and "Respuesta Útil). Also be aware that when someone includes an attachment in a response you will not find it in the inbox either.

Thank you!

/Jorge Gonzalez