In the PE 10.4 (which I have access to via KDS 1.1.1) I cannot find a means of seeing the "details" in the Resources view of the CPU component:
In the v10.3 (available in CW 10.6) I can see these details in a third column as can be seen in the figure below:
Is this a change in the design and this information is now presented in another place?
Regards,
--
Cesar Rabak
已解决! 转到解答。
Hello Cesar:
It seems that the new Tabs view is missing those details. But you can disable the Tabs_view and go back to classic, like this:
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Cesar:
It seems that the new Tabs view is missing those details. But you can disable the Tabs_view and go back to classic, like this:
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jorge Gonzalez!
Yep! There it is!
Thank you very much!
Now if I could find where is the Correct Answer button :smileyconfused:. Maybe because I see the interface in a non English locale this doesn't appear?
Hi Cesar:
I'm glad it helped :smileyhappy:.
That is your inbox. Inbox only shows an overview of the thread, but to access the complete thread you have to click on the thread title. Then you can see the "Correct Answer" and "Helpful Answer" buttons (or in your case "Respuesta Correcta" and "Respuesta Útil). Also be aware that when someone includes an attachment in a response you will not find it in the inbox either.
Thank you!
/Jorge Gonzalez