Configuring Master SPI Bus Speeds via PEx?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Configuring Master SPI Bus Speeds via PEx?

跳至解决方案
2,432 次查看
tharonhall
Contributor IV

I am using a K22F part and I need to configure the SPI bus in Master mode. In PEx under KDS, when I go to the spiCom1 component, and under the "Master mode" tab I can setup bus configurations. There is a "Clock rate" column that allows one to set up the clock rate. You can click on the value shown and get an button that takes you to a "Timing dialog - spiCom1/Clock rate" window. You can choose values based on 5 clock configurations. However, I don't know what is setting those clock configurations, and anything above 2.14MHz gives me an error, even though higher frequencies are listed.

I suspect I need to tweak the clock configurations, but I cannot locate where they are set. The modules references an fsl_clock_manager, but when I go there I don't see anything that actually sets up clock configurations.

Can anyone tell me where those are set up?

Thanks!

标记 (3)
0 项奖励
回复
1 解答
2,211 次查看
tharonhall
Contributor IV

OK, for anyone that might read this one, I figured this out today:

I created my project from an example project for the K22F Freedom board. For whatever reason, the project came with several clock configurations. I switched the init clock config to the fast runtime configuration and away things went. That was all fine and good, but I still couldn't get the SPI bus above 2.1 MHz.

It turns out that even though I was only using the one clock configuration, the PEx SPI module, in its desire to be helpful, freaked out that there were clock configurations that would not work with the higher speeds if I chose to use it. Now, I disagree with that approach since I could have clock configurations that I might run that I would NOT use SPI on, and PEx was denying me the opportunity.

Rather than risk anything breaking by deleting any of the unused clock configurations, I simply set them all to high speed and viola, I can now clock at much higher frequencies. :smileyhappy:

Of course, none of this helps explain why my soft SPI code is SO unbelievably slow. :smileysad:

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,209 次查看
dereksnell
NXP Employee
NXP Employee

Hi Tharon,

The clock configurations are part of the properties in the CPU component, and define the system clock frequencies used by the core and peripherals.  See screenshot below

Attached is a hands-on lab I created recently, dealing with the clock configurations within Processor Expert, and how it relates to peripheral setup. This lab was written for the IAR toolchain, but the Processor Expert steps are the same for any toolchain, including KDS.  So you can ignore the section on the IAR project.

Thanks


Clock Configs.jpg

2,212 次查看
tharonhall
Contributor IV

OK, for anyone that might read this one, I figured this out today:

I created my project from an example project for the K22F Freedom board. For whatever reason, the project came with several clock configurations. I switched the init clock config to the fast runtime configuration and away things went. That was all fine and good, but I still couldn't get the SPI bus above 2.1 MHz.

It turns out that even though I was only using the one clock configuration, the PEx SPI module, in its desire to be helpful, freaked out that there were clock configurations that would not work with the higher speeds if I chose to use it. Now, I disagree with that approach since I could have clock configurations that I might run that I would NOT use SPI on, and PEx was denying me the opportunity.

Rather than risk anything breaking by deleting any of the unused clock configurations, I simply set them all to high speed and viola, I can now clock at much higher frequencies. :smileyhappy:

Of course, none of this helps explain why my soft SPI code is SO unbelievably slow. :smileysad:

0 项奖励
回复
2,209 次查看
tharonhall
Contributor IV

Thanks, Derek. This threw me as I would have expected the clocks in a clock peripheral of some kind, so thank you for pointing me in the right direction. I did some quick and dirty tweaks and couldn't get the speed shifted up but now that I know where to look I am sure I can unravel the mystery.

Thanks again!

0 项奖励
回复