Can't choose SCI1 device on MagniV Device (S12ZVCA)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't choose SCI1 device on MagniV Device (S12ZVCA)

Jump to solution
756 Views
jer
Contributor II

I'm trying to set up a project for the S12ZVCA processor and can't seem to set up the SCI1 peripheral in processor expert, it's not a selectable option in processor expert.  If I don't choose anything under device, then I can select the RX1 and TX1 pins, but then I get the error about not having a device selected and can't generate the code or make an interrupt, when I try and choose a device, there is not SCI1 option and then the RX1 and TX1 pins are gone. I'm using Codewarrior 10.7.0

Thanks,

Labels (1)
0 Kudos
1 Solution
422 Views
jer
Contributor II

Found the issue.  The 48pin part does not have the SCI1 port, only SCI0.  The weird part is, in the datasheet the signals for RXD1 and TXD1 are still on there despite being non-existent, hence why I wired signals to them.

View solution in original post

0 Kudos
2 Replies
422 Views
aaronlee
Contributor V

Fixed the issue of Processor Expert in CodeWarrier v11.0

0 Kudos
423 Views
jer
Contributor II

Found the issue.  The 48pin part does not have the SCI1 port, only SCI0.  The weird part is, in the datasheet the signals for RXD1 and TXD1 are still on there despite being non-existent, hence why I wired signals to them.

0 Kudos