Asynchronical serial: unable to read values 0x00 with PE routine

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Asynchronical serial: unable to read values 0x00 with PE routine

1,086 Views
juanignaciotroi
Contributor III

Hello

With the KE02 on CW IDE I'm trying to implement an RS232 component using the asynchronical serial component provided with the processor expert.

Having had enabled interrupts, and within the ISR calling the function <AS1_RecvChar> - generated by the processor expert - I am able to read any type of character with the exception the character NULL (0x00). 

Is there any reason why this may happen? Could it be that the interrupt is never called when a NULL is on the Rx?

Kind regards, 

Juan Ignacio Troisi

0 Kudos
Reply
1 Reply

968 Views
juanignaciotroi
Contributor III

Can anyone help me with this issue?

0 Kudos
Reply