Async Serial: GetCharsInRxBuf never > 0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Async Serial: GetCharsInRxBuf never > 0

1,328 次查看
pklammer
Contributor II

What is wrong with the following picture??? It spits out "Hello World" but never receives any of my typing to echo!

int main(void)

/*lint -restore Enable MISRA rule (6.3) checking. */

{

    static unsigned char bUARTdebugInputCount = 0 ;

    LDD_TDeviceData * pUARTdebugDeviceDataStructure ;

    char strHelloWorld[] = "Hello, World!\r\nLEDsAsynchroSerial here!\r\n" ;

    byte bReceivedByte ;

    unsigned uCharsInRxBuf ;

    /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/

    PE_low_level_init();

    /*** End of Processor Expert internal initialization.                    ***/

    /* Write your code here */

    pUARTdebugDeviceDataStructure = ASerialLdd1_Init( NULL );

    ASerialLdd1_SendBlock( pUARTdebugDeviceDataStructure, strHelloWorld, sizeof( strHelloWorld ) ) ;

    for(;;) {

        while( ( uCharsInRxBuf = UARTdebug_GetCharsInRxBuf() ) > 0 ) {

            ++bUARTdebugInputCount ;

            UARTdebug_RecvChar( &bReceivedByte ) ;

            UARTdebug_SendChar( bReceivedByte ) ;

        }

    }

标签 (1)
0 项奖励
4 回复数

543 次查看
pklammer
Contributor II

While waiting for help, I'm tracing code to see if I can figure it out myself ...

Following examples and documentation and help as best I could, I coded the line ...

         pUARTdebugDeviceDataStructure = ASerialLdd1_Init( NULL );

... not least because I needed that pointer-to-structure initialized to use on the next line for the SendBlock call.

BUT!

I am very surprised to find, in Cpu.c/void PE_low_level_init(void) ...

     {

          [...]

          /* ### Asynchro serial "UARTdebug" init code ... */

          UARTdebug_Init();

          __EI();

     }

... and in void UARTdebug_Init(void) ...

     {

          [...]

          ASerialLdd1_DeviceDataPtr = ASerialLdd1_Init(NULL); /* Calling init method of the inherited component */

          HWEnDi();                            /* Enable/disable device according to status flags */

     }

In other words, I'm calling ASerialLdd1_Init() but PEx Generatded_Code is calling ASerialLdd1_Init(), too?

That doesn't seem right; is it?

0 项奖励

543 次查看
Lukas_Heczko
NXP Employee
NXP Employee

Hi,

I assume you are using the AsynchroSerial component. This one inherits Serial_LDD component and uses it as an interface to the hardware – the AsynchroSerial component on Kinetis families is rather SW wrapper to support migration from families where LDD components were not supported.

I’m not very familiar with serial communication drivers, however from the code snippet you posted it looks like you are using both Serial_LDD and AsynchroSerial methods at the same time – I guess this is source of your problems. You have to use either the AsynchroSerial component and its API or the Serial_LDD component (without the AsynchroSerial) and its API – it is not possible to use both of them for the same UART device.

Lukas

543 次查看
pklammer
Contributor II

This is a tough way to learn Processor Expert -- after-the-fact do-over, after I got it working "the wrong way"!

All I know so far is, there is a list of components in the right-hand panel of eclipse, and none of them are marked "deprecated" or "API" or "wrapper" or "migration".  So how are we to know -- before we waste time on the wrong ones -- which are the recommended components for application development, and which are "dependent" components that get pulled in automatically, and which are "legacy" components not recommended for new projects?

0 项奖励

543 次查看
Petr_H
NXP Employee
NXP Employee

I agree that the selection of the right component can be confusing for non-experienced Processor Expert users.

We are planning  improvements in the component library and its documentation to ease this task.

best regards

Petr Hradsky

Processor Expert Support Team

0 项奖励