Are PEx visual tools supported by IAR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Are PEx visual tools supported by IAR

跳至解决方案
1,523 次查看
christophertsch
Contributor III

We are evaluating the IAR tool and I see no obvious support for processor expert tools such as the component inspector and component library in any of the documentation related to IAR or KSDK for IAR. Is there any add-on for IAR tool for processor expert? Is there definitive documentation on how IAR works with Kinetis MCU's with respect to KSDK or processor expert?

THANKS!

标记 (4)
0 项奖励
回复
1 解答
1,332 次查看
BlackNight
NXP Employee
NXP Employee

Because IAR is not Eclipse based, these views do not exist in the IAR Embedded workbench.

How Processor Expert works with IAR is with the Driver Suite, see http://mcuoneclipse.com/2013/01/31/tutorial-iar-freertos-freedom-board/

Later version of IAR tools have even improved the support, see IAR ARM v6.7 comes with improved Processor Expert Support | MCU on Eclipse

There is as well a way to use the IAR compiler with Eclipse, with a plugin IAR provides (I have not tried it out recently, but that one should still apply):

http://mcuoneclipse.com/2013/11/03/tutorial-replacing-iar-ew-with-eclipse-ide/

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,333 次查看
BlackNight
NXP Employee
NXP Employee

Because IAR is not Eclipse based, these views do not exist in the IAR Embedded workbench.

How Processor Expert works with IAR is with the Driver Suite, see http://mcuoneclipse.com/2013/01/31/tutorial-iar-freertos-freedom-board/

Later version of IAR tools have even improved the support, see IAR ARM v6.7 comes with improved Processor Expert Support | MCU on Eclipse

There is as well a way to use the IAR compiler with Eclipse, with a plugin IAR provides (I have not tried it out recently, but that one should still apply):

http://mcuoneclipse.com/2013/11/03/tutorial-replacing-iar-ew-with-eclipse-ide/

I hope this helps,

Erich

0 项奖励
回复
1,332 次查看
christophertsch
Contributor III

Erich, thanks for your speedy response.

I have a follow up question. The first link uses CodeWarrior to somehow generate this Driver Suite. Can I use KDS to do the same thing? Are there any special instructions to do so?

Thanks!

0 项奖励
回复