Are KSDK based PEx components "released" independent of the KSDK release cycle?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Are KSDK based PEx components "released" independent of the KSDK release cycle?

1,155 次查看
jeffreygraves
Contributor III

Are KSDK based PEx components "released" independent of the KSDK release cycle?

If so, is there an update site similar to the Freescale KDS update site?

(http://freescale.com/lgfiles/updates/Eclipse/KDS)

标记 (4)
1 回复

901 次查看
vfilip
NXP Employee
NXP Employee

Hello,

no, they are tight to KSDK. Actually PEx is tool to provide easy configuration of KSDK. PEx components now handles corresponding drv files, compiler options, etc... Above this are supported PEx features like timing, validation, pin selection, design time preprocess, etc... PEx components (eclipse update) are stored in tools directory.

www.freescale.com/kpsdk

Best regards

Vojtech Filip

Processor Expert Support Team