Are KSDK based PEx components "released" independent of the KSDK release cycle?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are KSDK based PEx components "released" independent of the KSDK release cycle?

1,074 Views
jeffreygraves
Contributor III

Are KSDK based PEx components "released" independent of the KSDK release cycle?

If so, is there an update site similar to the Freescale KDS update site?

(http://freescale.com/lgfiles/updates/Eclipse/KDS)

Tags (4)
1 Reply

820 Views
vfilip
NXP Employee
NXP Employee

Hello,

no, they are tight to KSDK. Actually PEx is tool to provide easy configuration of KSDK. PEx components now handles corresponding drv files, compiler options, etc... Above this are supported PEx features like timing, validation, pin selection, design time preprocess, etc... PEx components (eclipse update) are stored in tools directory.

www.freescale.com/kpsdk

Best regards

Vojtech Filip

Processor Expert Support Team