Are KSDK based PEx components "released" independent of the KSDK release cycle?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are KSDK based PEx components "released" independent of the KSDK release cycle?

1,075件の閲覧回数
jeffreygraves
Contributor III

Are KSDK based PEx components "released" independent of the KSDK release cycle?

If so, is there an update site similar to the Freescale KDS update site?

(http://freescale.com/lgfiles/updates/Eclipse/KDS)

タグ(4)
1 返信

821件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

no, they are tight to KSDK. Actually PEx is tool to provide easy configuration of KSDK. PEx components now handles corresponding drv files, compiler options, etc... Above this are supported PEx features like timing, validation, pin selection, design time preprocess, etc... PEx components (eclipse update) are stored in tools directory.

www.freescale.com/kpsdk

Best regards

Vojtech Filip

Processor Expert Support Team