Android BSP building for i.mx8, imx-android-11.0.0_2.2.0.tar.gz download link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android BSP building for i.mx8, imx-android-11.0.0_2.2.0.tar.gz download link

4,002 Views
jomonthomas
Contributor I

Currently i am trying to build Android BSP, using Android™ User's Guide, Rev. android-11.0.0_2.2.0. But i could't find the Android release package imx-android-11.0.0_2.2.0.tar.gz. Where from i can download this package?

0 Kudos
Reply
8 Replies

3,849 Views
Jack-Cha
Contributor V

Thanks for quick clarification.

3,848 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You are welcome~~

Wish you have a nice day

3,863 Views
Jack-Cha
Contributor V

Hi

the script of imx_android.setup.sh works now when it's executed from ~/. location instead of inside ~/imx_xxxx directory.

 

BTW. Is the repo sync related with python version installed? Should I set default python version to 3.6 on Ubuntu 18.4.5?

Thanks.

Regards, 

Jack

0 Kudos
Reply

3,854 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

No, recommend you to use the default one.

3,876 Views
Jack-Cha
Contributor V

Hi NXP

I am trying to setup the Android source code version 11.0.0.2.2.0 on top of Ubuntu 18.4.5_x64.

I have followed the instruction according to Android User Guide, But there're lots of fetch error.

Can you please let us know the setup instruction that work fine?

Regards, 

Jack

 

0 Kudos
Reply

3,855 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

For build android BSP you can follow the user guide we supply,

To build the Android source files, use a computer running the Linux OS. The Ubuntu 18.04 64-bit version is the most tested
environment for the Android 11.0 build.
To synchronize the code and build images of this release, the computer should at least have:
• 450 GB free disk space
• 16 GB RAM

 In addition to the packages requested on the Android website, the following packages are also needed in our user guide.

 

3,988 Views
Rita_Wang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

3,875 Views
Jack-Cha
Contributor V

Hi

I already followed the same link download and user guide. 

It doen not work even I followed the same instruction that was written in User Guide. 

Can you please specify the pre-requisite of build envioronment?

Thanks.

Tags (1)
0 Kudos
Reply