Android BSP building for i.mx8, imx-android-11.0.0_2.2.0.tar.gz download link

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android BSP building for i.mx8, imx-android-11.0.0_2.2.0.tar.gz download link

4,112 次查看
jomonthomas
Contributor I

Currently i am trying to build Android BSP, using Android™ User's Guide, Rev. android-11.0.0_2.2.0. But i could't find the Android release package imx-android-11.0.0_2.2.0.tar.gz. Where from i can download this package?

0 项奖励
回复
8 回复数

3,959 次查看
Jack-Cha
Contributor V

Thanks for quick clarification.

3,958 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

You are welcome~~

Wish you have a nice day

3,973 次查看
Jack-Cha
Contributor V

Hi

the script of imx_android.setup.sh works now when it's executed from ~/. location instead of inside ~/imx_xxxx directory.

 

BTW. Is the repo sync related with python version installed? Should I set default python version to 3.6 on Ubuntu 18.4.5?

Thanks.

Regards, 

Jack

0 项奖励
回复

3,964 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

No, recommend you to use the default one.

3,986 次查看
Jack-Cha
Contributor V

Hi NXP

I am trying to setup the Android source code version 11.0.0.2.2.0 on top of Ubuntu 18.4.5_x64.

I have followed the instruction according to Android User Guide, But there're lots of fetch error.

Can you please let us know the setup instruction that work fine?

Regards, 

Jack

 

0 项奖励
回复

3,965 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

For build android BSP you can follow the user guide we supply,

To build the Android source files, use a computer running the Linux OS. The Ubuntu 18.04 64-bit version is the most tested
environment for the Android 11.0 build.
To synchronize the code and build images of this release, the computer should at least have:
• 450 GB free disk space
• 16 GB RAM

 In addition to the packages requested on the Android website, the following packages are also needed in our user guide.

 

4,098 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport
0 项奖励
回复

3,985 次查看
Jack-Cha
Contributor V

Hi

I already followed the same link download and user guide. 

It doen not work even I followed the same instruction that was written in User Guide. 

Can you please specify the pre-requisite of build envioronment?

Thanks.

标记 (1)
0 项奖励
回复