9S08MP16 Flash (reserve a partition for system fault)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

9S08MP16 Flash (reserve a partition for system fault)

2,796 Views
kazbi
Contributor I

 

Hello,  

 I´m using the DEMO9S08MP16 (16KB Flash) on my prototype with Code Warior Processor Expert and I would like to use some adresses for my fault handling.

So as following, I choose the adresses( 0xFA00, 0xFA01...).

 

#define DLK_V_Warning()       IFsh1_SetByteFlash(0xFA00,10)
#define DLK_V_Fault()         IFsh1_SetByteFlash(0xFA00,11)
 

#define DLK_T_Fault()         IFsh1_SetByteFlash(0xFA01,11)
#define DLK_T_Warning()       IFsh1_SetByteFlash(0xFA01,10)

 

When a fault (B) or warning(A) occurs it schould be saved wtih the defined function.

 

My Problem:  

I don´t know how I can reserve some adresses for my fault and warning handling witout perturbing my realtime program in the flash. 

 

 

Best regards

 

kazbi

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

2,548 Views
ProcessorExpert
Senior Contributor III

Hello,

I think that better way will be to set your flags to end of non-volatile memory, that means exactly to 0xFFAC and 0xFFAD and after that exclude this area from linking process of your regular code using the following steps:

- go to the build options tab in CPU component
- Set Size of the Memory Area0 (Name: ROM) to 3FAC

best regards
Vojtech Filip
Processor Expert Support team

2,548 Views
kazbi
Contributor I

Thank you  Filip,

 

I try your konfiguration, but I in  the non-volatile memory is only 00 in all reserved adresses.

I don´t see the fault or Warning??

 

I have 10 Fault and I set the memory area0 size to 3FA4.

so it beginn from 0xFFA4 to 0xFFAD.

 

#define D_V_Warning()       IFsh1_SetByteFlash(0xFFA4,10)
#define D_V_Fault()         IFsh1_SetByteFlash(0xFFA4,11)
 

#define D_T_Fault()         IFsh1_SetByteFlash(0xFFA5,11)
#define D_T_Warning()       IFsh1_SetByteFlash(0xFFA5,10)


#define D_L_Fault()  IFsh1_SetByteFlash(0xFFA6,11)


#define D_C_Fault()         IFsh1_SetByteFlash(0xFFA7,11)
#define D_C_Warning()       IFsh1_SetByteFlash(0xFFA7,10)


#define B_V_Fault()        IFsh1_SetByteFlash(0xFFA8,11)
#define B_V_Warning()      IFsh1_SetByteFlash(0xFFA8,10)


#define B_T_Fault()        IFsh1_SetByteFlash(0xFFA9,11)
#define BORD_T_Warning()      IFsh1_SetByteFlash(0xFFA9,10)


#define B_Ion_Fault()      IFsh1_SetByteFlash(0xFFAA,11)    

#define B_Ioff_Fault()     IFsh1_SetByteFlash(0xFFAB,11)

#define INF_Fault()        IFsh1_SetByteFlash(0xFFAC,11)

#define PYRO_Fault()      IFsh1_SetByteFlash(0xFFAD,11)

 

Best Regards

Kazbi

0 Kudos
Reply