Vboost using PWM (manual) NOT hysteretic

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Vboost using PWM (manual) NOT hysteretic

4,959 次查看
Fast
Contributor V

Has anyone firmware code for SD6 MC33816 PT2000 or PT2001, using manual or PWM control of Vboost DCDC generator as promised in; fact-sheet/PT2000A4FS.pdf ? Only guidance is it should be like injector code, but is only low side, and needs voltage as well as current control.

标签 (1)
标记 (1)
0 项奖励
回复
9 回复数

4,733 次查看
Fast
Contributor V

I am good for now. Yes the attachment shows the "manual" method for Vboost generation where microcode turns LS7 on and off.

Shall we close? Any other questions?

0 项奖励
回复

4,931 次查看
guoweisun
NXP TechSupport
NXP TechSupport

HI Fast

 All of these parts software are list here:

guoweisun_0-1736732852841.png

PT2000 3/4/6 Cylinders Engine Evaluation Board | NXP Semiconductors

 

Hope this could help you!

 

BR

0 项奖励
回复

4,901 次查看
Fast
Contributor V

For PT2001 see my solution attached, please critique .

@guoweisun @RafaR 

 

标记 (1)
0 项奖励
回复

4,877 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Could you please introduce or explain your code detail here?

0 项奖励
回复

4,859 次查看
Fast
Contributor V

Sure the reason see "PT2001 why inhibit Vboost?"

So there is an inner loop doing the PWM, if Vboost is low, with a limit for the On time. Direct control of LS7, no async hardware used, that may be susceptible to noise. Usual switch off is when current is reached. Then a coast down Off time. When Vboost target reached  the outer loop rests, till Vboost is too low.

Note the is no Vboost inhibit, as not needed see referenced post.

Code use at own risk!

标记 (1)
0 项奖励
回复

4,757 次查看
guoweisun
NXP TechSupport
NXP TechSupport

guoweisun_0-1737510763987.png

But we implement Vboost using both sync and async modes

I didn't understand what you said, and I didn't know if it was a function inside our chip or some other way

0 项奖励
回复

4,744 次查看
Fast
Contributor V

Hi guoweisun

Yes there is some built in hardware, for PT2001/MC33816 only LS7 has this feature that is called VFM variable frequency mode, or hysteretic current control , or async phase. For a reason I do not entirely understand, this mode has issues, either this mode is sensitive to disturbances in Vboost from current drained by a load, or the current control of load supplied from Vboost. Apparently not sensitive if reservoir capacitor is taken directly to ground, avoiding Vboosts current sense.  It maybe booth. The manual PWM mode coded has avoided that condition. Multiple names for same feature often makes these powerful solenoid controllers seem unnecessarily complex, but persist you will be rewarded. Sync phase is essentially Off that sounds much simpler to me.

Fast_0-1737539689581.png

 

标记 (1)
0 项奖励
回复

4,730 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Please directly send mail to lex.liu@nxp.com ,I always discussed with him for this topic.

0 项奖励
回复

4,732 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Does your above description have any relationship with your said manual PWM?

0 项奖励
回复