[PT200x] Vds disable window

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[PT200x] Vds disable window

1,647 Views
erichong
NXP Employee
NXP Employee

Hello,

May I ask you one question regarding some effect of Vds disable window?

I'm answering to a question which is coming from Autron during the short to GND/Batt test.

And here are some questions need your advice.

 

Question A)

1) Assume now I'm in current hold phase and HS1 driver (Vbat for FET) repeats turning on/off. Diag is enabled.

2) At the moment when HS1 is off in the middle of hold phase, Vsrc of HS1 short to GND occurred.

3) But before expiration of filter length, HS1 is turned on again.

The question is, does the uCore detects Vds fault only after disable window time triggered by HS1 turn on command?

 

Question B)

I tried to understand how the disable window works for Vds monitoring in the PSC simulator but could not fine a good internal signal showing the operation of disable window. Please let me know which signal I have to monitor.

 

Thank you,

Eric

Labels (1)
0 Kudos
Reply
3 Replies

1,636 Views
philippe_meunie
NXP Employee
NXP Employee

Bonjour Eric,

For Question A) the fault will not be detected as disable window has been reset when HS state has changed (according to description in application note AN12336, page 28 :

pastedImage_1.png

Cordially,

Philippe

0 Kudos
Reply

1,635 Views
pierrecalmes
NXP Employee
NXP Employee

Hi Eric,

For question B see example of signals that customer can look at on simulator:

pastedImage_1.png

The key is to look at the VDS counter for the dedicated High Side or Low side and teh status VDS showing when start to count and when VDS enabled (meaning disable windows is fnished)

You can load file attached to have access to the signals.

Let me know if any issue,

Regards

Pierre

0 Kudos
Reply

1,635 Views
erichong
NXP Employee
NXP Employee

Thank you, Pierre.

StatusVds and WindowCounterVds explain the situation.

Best Regards,

Eric 

0 Kudos
Reply