PT2001 Vboost shortcut questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PT2001 Vboost shortcut questions

ソリューションへジャンプ
2,385件の閲覧回数
Fast
Contributor V

PT2001SWUG Rev 3.0 says "Note that in order to use the async or sync mode, the low-side use for DCDC has to be set as shortcut 2 (ex: dfsct undef ls7 undef). "

Yet no examples of firmware use that line of code. Is statement true, is it another hangover from PT2000?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,322件の閲覧回数
Fast
Contributor V
Yes close. Can you link these conversations. I do not want to "fall between two stools", I am surprised that this is a new question, considering the age of the MC33816. Please pick up the "baton", RafaR. Sorry for the English idioms.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,351件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi Fast

Could you please give more explain about your issue/questions? That's difficult for understanding!

0 件の賞賛
返信
2,341件の閲覧回数
Fast
Contributor V

Good morning guoweisun,


Please see the conversation with RafaR.

I am looking for guidance on DCDC code using the PWM mode ( AKA manual mode) , all microcode. That is not using the resonant mode since PT2001 cannot support on LS7 as no Vds sensing. I am led to believe that in PWM mode, and with Vboost capacitor grounded, so Vboost not effected by Iboost phase at injector which disturbs current control.

タグ(1)
0 件の賞賛
返信
2,331件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi Fast

Since Rafael Rojas supported to you before please directly contact with him for continuous support.

Rafael is my colleague I think he will help you continuously.

Thanks!

 

0 件の賞賛
返信
2,323件の閲覧回数
Fast
Contributor V
Yes close. Can you link these conversations. I do not want to "fall between two stools", I am surprised that this is a new question, considering the age of the MC33816. Please pick up the "baton", RafaR. Sorry for the English idioms.
0 件の賞賛
返信
2,263件の閲覧回数
Fast
Contributor V
See Vboost using PWM (manual) NOT hysteretic. Set LS7 Slewrates to max, very clean waveforms at 100kHz
0 件の賞賛
返信