Dependencies of actuator window and wave window of MC33816 simulator software ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dependencies of actuator window and wave window of MC33816 simulator software ?

1,704 Views
agkulkarni94
Contributor I

Hello,

If an actuator is removed from the actuator window then output waveform of the corresponding actuator get disappear from the wave window, and it happens only for some actuators and not for all. So how actuator window and wave window are dependent on each other ?.

Labels (1)
0 Kudos
Reply
1 Reply

1,650 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

According to the datasheet:

If the disable window is exceeded, and the automatic diagnosis detects an error between the HSx_in and the filtered HSx_Vds_fbk signal, an interrupt is generated towards the microcore. Due to this interrupt the program counter of the microcore is set to the first instruction of the error routine. It takes four ck cycles (666 ns at 6.0 MHz) until the execution of the first microcode operation of the error routine is completed. It means that if the first microcode command is used to switch off all pre-drivers, this action is delayed by four ck cycles. In more detail, it takes one ck cycle to detect the error, one ck cycle to generate the interrupt, one ck cycle to move the program counter to the error routine and one ck cycle to execute the first instruction.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply