p2020是否支持 ELBC与DDR之间DMA传输

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

p2020是否支持 ELBC与DDR之间DMA传输

1,005 Views
Jaygao
Contributor I

p2020_dma.PNG

0 Kudos
Reply
2 Replies

959 Views
June_Lu
NXP TechSupport
NXP TechSupport

13.4.2 DMA transfer interfaces
The DMA can be used to achieve data transfers across the entire memory map.
Note that a single DMA transfer in any of the direct or chaining modes must not cross a
16 GB (34-bit) address boundary.

0 Kudos
Reply

781 Views
Jaygao
Contributor I

is the external request need for the DMA transcation between e LBC and ddr?

0 Kudos
Reply