mpc8548 boot failure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mpc8548 boot failure

917 次查看
nit
Contributor I

hello every one....

I am facing a problem in customized mpc8548 board. please help me.

We are using a customized mpc8548 board. After loading

flash the processor is not booting i checked the CS0# signal on

power on, it was always high. Although the same code is running

through Code Warrior jtag prob and it is generating CS0# signals

where i got a pulse train. And this running code is ROM version

which i selected in JTAG CW tool without any initialization file.

But when i loaded the elf file of same code into the flash. there

was no CS0# signal appearing. Please suggest. Is it related to

some start up code problem? Please tell us.

标记 (3)
0 项奖励
回复
1 回复

735 次查看
lunminliang
NXP Employee
NXP Employee
0 项奖励
回复