ltib networking problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ltib networking problem

976 次查看
ssssss
Contributor II

hi

i have an mpc8568 eval board and i configured a linux kernel for it with ltib.

i tested several configurations in ltib but in no one i recieved a working networking system (the device couldn't ping anything on the network and doesn't have /etc/interfaces or ...)

i tried changing ip address manually, adding dhcp support and trying several setting in the linux but the result not changed so i used wireshark to catch output packets and there was some output but no arp or dhcp packets and in fact no ip packets.

plz help me

thanks

mohammad

标记 (3)
0 项奖励
回复
1 回复

904 次查看
alexander_yakov
NXP Employee
NXP Employee

1. Which board you are using? Please specify board name or exact partnumber

2. Which BSP you are using? Please specify BSP file name and where it was downloaded

3. What happens if you burn pre-built binary image, which is typically supplied in BSP?

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复