ltib networking problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ltib networking problem

978件の閲覧回数
ssssss
Contributor II

hi

i have an mpc8568 eval board and i configured a linux kernel for it with ltib.

i tested several configurations in ltib but in no one i recieved a working networking system (the device couldn't ping anything on the network and doesn't have /etc/interfaces or ...)

i tried changing ip address manually, adding dhcp support and trying several setting in the linux but the result not changed so i used wireshark to catch output packets and there was some output but no arp or dhcp packets and in fact no ip packets.

plz help me

thanks

mohammad

タグ(3)
0 件の賞賛
返信
1 返信

906件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

1. Which board you are using? Please specify board name or exact partnumber

2. Which BSP you are using? Please specify BSP file name and where it was downloaded

3. What happens if you burn pre-built binary image, which is typically supplied in BSP?

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信