linux application build in LTIB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

linux application build in LTIB

1,196件の閲覧回数
garimella
Contributor I

Using a custom Mpc83XX board. Was able to successfully build a device driver and generate rootfs. I wanted to know the following

1. How to build a linux application invoking device driver (basic compilation procedure from .ltib -m shell prompt not the source code)

2. How to run this application during start up. ( I do not want to load everytime)

3. Any sample application program code for ethernet communication for MPC83XX?

0 件の賞賛
返信
1 返信

1,072件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the following document:

http://ltib.org/pages/LTIB_generic_v1.4_-_version_6.4.1.pdf

This document contains example for developing and invoking device driver and sample application program.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信