is MPC8349 series with cryptography technique?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

is MPC8349 series with cryptography technique?

ソリューションへジャンプ
2,092件の閲覧回数
jimmycheung1218
Contributor I

It is a layman question. Could anyone tell if model MPC8349EVVAJFB is designed or modified to use cryptography employing digital techniques performing cryptographic function?

I need such information to report to the government so as to get a import license.

attached it is the form i need to fill in.

0 件の賞賛
返信
1 解決策
2,000件の閲覧回数
bpe
NXP Employee
NXP Employee

The part you mentioned is equipped with on-chip cryptography hardware accelerator.

Details can be found in the chip Reference Manual, Chapter 14. Visit the link below to

obtain the document.

PowerQUICC II Pro Processor with DDR2, Dual P|NXP


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,001件の閲覧回数
bpe
NXP Employee
NXP Employee

The part you mentioned is equipped with on-chip cryptography hardware accelerator.

Details can be found in the chip Reference Manual, Chapter 14. Visit the link below to

obtain the document.

PowerQUICC II Pro Processor with DDR2, Dual P|NXP


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,000件の閲覧回数
jimmycheung1218
Contributor I

Well, in this case i will have to fill-in the long questionnaire to the government. :smileycry:

Thanks so much.

0 件の賞賛
返信