i2c bus busy problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i2c bus busy problem

3,258 Views
love_hate_and_repeat
Contributor III

i'm working on t1042 cpu and i didnt solve some problems i encountered. 

i firstly send start condition to bus and after that, i dont send anything except stop condition to free bus but 

after start condition, if i send stop condition to bus, it doesnt work and bus is always remaining as busy.

code is like follow; 

send start condition

send stop condition

exit

0 Kudos
Reply
3 Replies

2,830 Views
jeffthompson
Contributor V

Try reconfiguring the clock as a GPIO pin, toggle it 16 times, then configure it back to an I2C clock and try again.

See Common Problems In Systems - I2C Bus. Got to Analyzing Obscure Problems/Blocked I2C Bus.

0 Kudos
Reply

2,830 Views
Pavel
NXP Employee
NXP Employee

See the Section 23.5.3.1 of the T1042 Reference Manual:

The bus is detected to be busy upon the detection of a START condition, and idle upon the detection of a STOP condition.

It looks like that a STOP condition is not detected.

Send STOP condition again.

 

Try to use command sequence from the Section 23.6.2.3.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,830 Views
love_hate_and_repeat
Contributor III

thanks.

0 Kudos
Reply