how to write data into m58bw016fb ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to write data into m58bw016fb ?

2,898 次查看
venkat1
Contributor III

hi folks,

 I am working on mpc8358e processor. In this i used m58bw016fb flash memory as a boot memory.  I am struct at writing a data into the memory (for config. RCWL and RCWH reg.) in hard code mode. Can you please help me how to write the data into this flash and also tel me what are the commands for write function.

thank you.

regards,

venkat d   

0 项奖励
回复
3 回复数

2,750 次查看
Pavel
NXP Employee
NXP Employee

See attached file.

This file contains documentation and example for adding new Flash to CodeWarrior 8.8 Flash Programmer.

Have a great day,
Pavel Chubakov

0 项奖励
回复

2,750 次查看
Pavel
NXP Employee
NXP Employee

NXP offers LTIB Linux BSP for the MPC8360MDS board.

See the following page:

https://www.nxp.com/products/processors-and-microcontrollers/legacy-mcu-mpus/powerquicc-processors/p...

 

This LTIB BSP supports u-boot boot loader.

See documentation for this BSP in the attached file.

See information about deployment in this document.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,750 次查看
venkat1
Contributor III

Thank you sir...

we wrote data on flash.Can you tell how to add flash device in code warrior 8.8 . flash is m58bw016fb (512kx32x1) memory.

Send me reference data similar for 8358 processor..

regards,

venkat. 

0 项奖励
回复