how to link mpc8247 60x bus with dualportram IDT7026?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to link mpc8247 60x bus with dualportram IDT7026?

633 Views
zzasia
Contributor II

how to link  mpc8247 60x bus  with  dualportram IDT7026?

then c language  take  the IDT7026 as RAM  and create  veriaty(read  and  write)  directly.

some device  link  with  the other side of dualportram IDT7026, need not  DMA  to DDR.

so  access  is  faster.

3 Replies

499 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

I suppose the MPC8247 is the only bus device in the system. I.e. it operates in single-MPC8247 bus mode, when the MPC8247 internal memory controller controls all devices on the external pins. As I can see IDT7026 looks like static ram with byte select signals which should be assigned during write and read. The GPCM cannot do that. So you should use UPM. Let we use bank n of the MPC8247 memory controller. Select UPM for the bank n. In this case you can connect MPC8247 and  IDT7026 in the next way:

MPC8247 – IDT7026

PCSn – CE

A[27:30] – A[0:13]

PBS[0:1] – UB,LB and D[0:15] – IO[15:0] (or

PBS[0:1] – LB, UB and D[0:15] – IO[0:15], check do you need byte swap with the second port)

PGPL1 – R/W

PGPL2 – OE

I do not see suitable solution for testing the IDT7026 BUSY signal by the MPC8247. Possibly you can use another the MPC8247 memory controller bank m for access to the IDT7026 semaphores (i.e. connect PCSm to the SEM input). Using semaphores in the software you can avoid simultaneous access to the same memory cell by left and right port.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

499 Views
zzasia
Contributor II

i found  :Tsm320   pin(RD) can  be linked  with IDT7026 pin(BUSY)

0 Kudos

499 Views
zzasia
Contributor II

and  i  read  a book  about  mpc5553 ,it  has  EBI, looks like  60X,    i think   maybe  BB(low) pin should link  with  IDT7026 BUSY(low  or  high?).

0 Kudos