hi
my demo board is P2020DS , i use the sdk1.6. I want use the p2020ds as NTP server , how to include the NTP server module and configuration? thank U.
root@p2020ds:~# date -R                                                         
Mon, 10 Aug 2020 10:13:11 +0000                                                 
root@p2020ds:~#                                                                 
root@p2020ds:~#                                                                 
root@p2020ds:~#                                                                 
root@p2020ds:~# ntpd                                                            
BusyBox v1.22.1 (2020-08-10 01:44:42 PDT) multi-call binary.                    
                                                                                
Usage: ntpd [-dnqNwl] [-S PROG] [-p PEER]...                                    
                                                                                
root@p2020ds:~#    
 yipingwang
		
			yipingwang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Please add "ntp" in IMAGE_INSTALL variable in meta-fsl-networking/images/fsl-image-core.bb.
IMAGE_INSTALL += " \
 packagegroup-fsl-core \
 ntp \
"
Then rebuild rootfs filesystem with the following command.
$ bitbake fsl-image-core
hi Yiping Wang
I have done as ur suggestion. but thers is no /etc/ntp.conf and how can I config p2020ds as NTP service ? c an u give me some suggestion?
root@p2020ds:/# service ntpd start                                              
-sh: service: command not found                                                 
root@p2020ds:/# 
/etc# ntp.conf                                                     
-sh: ntp.conf: command not found                                                
root@p2020ds:/etc#                                                              
root@p2020ds:/etc#                                                              
root@p2020ds:/etc#                                                              
root@p2020ds:/etc#                                                              
root@p2020ds:/etc#                                                              
root@p2020ds:/etc# cd ..                                                        
root@p2020ds:/# ntpd  -p 192.168.5.12 -qNn                                      
ntpd: time slew +0.000000s               
add
ntpd -p 192.168.1.16 -qNn
root@p2020ds:/# /etc/init.d/ntpd star
Starting ntpd: /usr/sbin/ntpd is already running                                
2415                                                                            
done                                                                            
root@p2020ds:/#  netstat -ln|grep 123                                           
udp        0      0 192.168.1.16:123        0.0.0.0:*                           
udp        0      0 127.0.0.1:123           0.0.0.0:*                           
udp        0      0 0.0.0.0:123             0.0.0.0:*                           
udp6       0      0 fe80::2e0:cff:fe02::123 :::*                                
udp6       0      0 ::1:123                 :::*                                
udp6       0      0 :::123                  :::*                                
root@p2020ds:/# ntpstat                                                         
-sh: ntpstat: command not found                                                 
root@p2020ds:/# 
 yipingwang
		
			yipingwang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Please execute the following commands.
/etc/init.d/ntpd restart
add problem, why service: command not found ? thank u.
 2409 ttyS0    00:00:00 sh                                                      
 2415 ?        00:00:00 ntpd                                                    
 2424 ttyS0    00:00:00 ps                                                      
root@p2020ds:/# service stop ntpd                                               
-sh: service: command not found                                                 
root@p2020ds:/#