Hi NXP Support Team,
please hlep me
I am using T2080 custom board with NOR Flash .I have code Warrior [CW_PA_v10.5.0] installed in my system.I want to program RCW/uboot into the nor flash,but always shows “Failed to reset the target”.What should I do?
1. Please refer to section "4.6.4.1.1 Hard Coded RCW Options" in T2080RM.pdf to configure the target board as hard-coded RCW mode.
2. Please refer to the following document to do flash programming with CodeWarrior for PA 10.5.1.
Please configure the target board as hard-coded RCW and don't use JTAG file override RCW function. And just use the default SRAM CodeWarrior project.
Because the JTAG file is only for T2080RDB demo board, you have to modify it according to your custom board.