hi! in MPC8308, can I dirrectly use one USB without PHY?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hi! in MPC8308, can I dirrectly use one USB without PHY?

749 Views
bsw_0204107
Contributor I

hi! in MPC8308, can I dirrectly use one USB without PHY?

0 Kudos
Reply
1 Reply

640 Views
Pavel
NXP Employee
NXP Employee

The MPC8308 USB ULPI cannot be connected to other USB ULPI controller. The MPC8308 USB ULPI control signals are inputs: USBDR_PWR_FAULT, USBDR_CLK, USBDR_DIR and USBDR_NXT. See the Table 13-1 of the MPC8308 Reference Manual.

It required using a USB ULPI PHY.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply