e500 core revision

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

e500 core revision

Jump to solution
1,856 Views
benjaminchauvel
Contributor I

Hello,

i was reading an interesting answer about Application Note AN3532 and CPU30 Erratum : https://community.nxp.com/message/435201?commentID=435201#comment-435201 

I'm looking for an official document describing e500 core revision for P2020 so i can do only step 2. 3. 4. and 5 for instruction cache parity error handling ( if i'm correct, I don't want to do a full cache invalidation ) .

An official answer on your forum may not be enough for QA department. Do you know where can i found that information ?

Thanks.

Benjamin

0 Kudos
Reply
1 Solution
1,780 Views
ufedor
NXP Employee
NXP Employee

P2020 silicon Rev 1.0 has e500 core Rev 4.0

P2020 silicon Rev 2.0 has e500 core Rev 5.0

P2020 silicon Rev 2.1 has e500 core Rev 5.1

From the P2020 QorIQ Integrated Processor Hardware Specifications, 4.2.1 Part Marking

P2020xtencdr

r - Silicon (die) revision:

A = Rev 1.0
B = Rev 2.0
C = Rev 2.1

View solution in original post

0 Kudos
Reply
2 Replies
1,780 Views
benjaminchauvel
Contributor I

thank you

0 Kudos
Reply
1,781 Views
ufedor
NXP Employee
NXP Employee

P2020 silicon Rev 1.0 has e500 core Rev 4.0

P2020 silicon Rev 2.0 has e500 core Rev 5.0

P2020 silicon Rev 2.1 has e500 core Rev 5.1

From the P2020 QorIQ Integrated Processor Hardware Specifications, 4.2.1 Part Marking

P2020xtencdr

r - Silicon (die) revision:

A = Rev 1.0
B = Rev 2.0
C = Rev 2.1

0 Kudos
Reply