codewarrior v8.8 + codewarrior tap issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

codewarrior v8.8 + codewarrior tap issue

1,225 Views
zbxggs
Contributor II

i used to program MPC8323 flash : codewarrior v8.8 + codewarrior tap(patch 8.8.6 is installed),there is no problem.

but recently ,i buy a new codewarrior tap ,i can't parogam flash .finally ,i fond the new one is rev H, the old one is rev G.

please help me ,how to program MPC8323 ,use codewarrior v8.8 with codewarrior tap rev H??

thanks.

0 Kudos
Reply
3 Replies

1,054 Views
LFGP
NXP TechSupport
NXP TechSupport

dear @zbxggs , 

I have asked to the internal team apps about your very last question, and they answer that the version H and the version G are the same, you don't have to worry about it. So, the procedure you must follow to flash the MPC  is the same in both version. 

please contact with the person you have purchased the CW TAP in order to start a guaranty   procedure or check with the distributor the error logs you are facing.

BR

LFGP

0 Kudos
Reply

1,205 Views
LFGP
NXP TechSupport
NXP TechSupport
Dear @zbxggs

Are you using Windows 7? you have to use it.
please share the CCS log, in order to get a clue about the issue, and please, share a picture of the new one CW TAP ( both sides please)
0 Kudos
Reply

1,056 Views
zbxggs
Contributor II

您好,如果我们想用codewarrior tap H版本,应该用哪个版本的codewarrior 替代8.8版本?

Tags (1)
0 Kudos
Reply