about T2080 SERDES MODE(SGMII)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about T2080 SERDES MODE(SGMII)

881 Views
王浩宇
Contributor I

When I configure some of the T2080 SEDES into SGMII, in addition to the hardware configuration of the SERDES mode, in the T2080 SDK, there are some files need to modify the configuration, so that T2080 can identify the external SGMII PHY

Labels (1)
0 Kudos
1 Reply

447 Views
ufedor
NXP Employee
NXP Employee

Yes, it is needed to have correct PHY connection type specified in the DTS:

phy-connection-type = "sgmii";

You could refer to the Linux sources repository:

sdk/linux.git - Freescale PowerPC Linux Tree

0 Kudos