Yocto jethro build system for MPC8309

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto jethro build system for MPC8309

1,699 Views
Sw2
Contributor I

Hi,

currently I am using yocto jethro build system for mpc8309.

I am facing some issues while building in ubuntu 20 latest Linux.

Can someone suggest which ubuntu version that  I can use?

0 Kudos
Reply
1 Reply

1,682 Views
Pavel
NXP Employee
NXP Employee

NXP offers LTIB Linux BSP for the MPC9309KIT board:

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=MPC8309-KIT_Linux_BSP

This BSP usually is used under Ubuntu 10 or Ubuntu 12.

 

NXP offers Yocto SDK for QorIQ processors:

https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/linux-sdk...

 

See the Sections 3.3.1, 3.3.2 and 3.3.5 abot customizing u-boot, kernel and root file system in SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

0 Kudos
Reply