Why MPC8306SOM using Flash m29W640gt ,but can't find the device in CW8.8 programmer device list.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why MPC8306SOM using Flash m29W640gt ,but can't find the device in CW8.8 programmer device list.

Jump to solution
1,872 Views
00lirui
Contributor I

   Why MPC8306SOM using Flash m29W640gt ,but can't find the device in CW8.8 programmer device list??

0 Kudos
Reply
1 Solution
1,740 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Li Rui,

It uses flash algorithm of M29W640DB, please refer to the template file in C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC\83xx, and which uses "amd" flash algorithm in C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC, you could find the information from C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC\FPDeviceConfig.xml.

Actually in your previous thread, I didn't think it was flash algorithm problem.

Would you please provide more detailed information in the previous thread?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,741 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Li Rui,

It uses flash algorithm of M29W640DB, please refer to the template file in C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC\83xx, and which uses "amd" flash algorithm in C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC, you could find the information from C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC\FPDeviceConfig.xml.

Actually in your previous thread, I didn't think it was flash algorithm problem.

Would you please provide more detailed information in the previous thread?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply