Whether a HDLC port can be configured to work in SDLC mode in QUICC engine of MPC8309?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Whether a HDLC port can be configured to work in SDLC mode in QUICC engine of MPC8309?

1,325 Views
priyadarshiniba
Contributor I

Does HDLC Controller of the QUICC engine supports SDLC transmission.

3 Replies

1,121 Views
priyadarshiniba
Contributor I

Thank you Serguei Podiatchev. Can you point me any link/QUICC manual for reference?.

0 Kudos
Reply

1,121 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

The HDLC controller of the QUICC engine supports SDLC transmission. The HDLC controller supports the frame structure which can be shared by HDLC and SDLC.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,121 Views
r8070z
NXP Employee
NXP Employee

You can download "QUICC Engine® Block Reference Manual with Protocol Interworking" from the MPC8309 page on NXP site

Low-Power PowerQUICC II Pro Processor with DDR2, e|NXP

0 Kudos
Reply