Where can I find MPC8548CDS_20060224-ltib.iso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I find MPC8548CDS_20060224-ltib.iso

Jump to solution
1,282 Views
albertandreasjr
Contributor II

Where can I find MPC8548CDS_20060224-ltib.iso.

This is referenced in the LTIB Quick Start: Targeting the MPC8548E CDS System, Document Number: AN3094.

I am interested in the UBoot and Linux source, and tool chain for the MPC8548E.

0 Kudos
Reply
1 Solution
1,038 Views
alexander_yakov
NXP Employee
NXP Employee

I do not see where "MPC8360E26_20081112-LTIB.iso" is mentioned in AN3094.pdf, I assume this is a typo, because MPC8360 BSP is not applicable to MPC8548E CDS board.

For MPC8548E CDS board please download BSP from this page:

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

5 Replies
1,038 Views
albertandreasjr
Contributor II

Yes you were correct.  I updated the question to refer to the correct BSP.

0 Kudos
Reply
1,038 Views
alexander_yakov
NXP Employee
NXP Employee

Thank you.

Please use most recent BSP downloaded from the link I mentioned in my previous reply.

0 Kudos
Reply
1,038 Views
albertandreasjr
Contributor II

Yes, I did; however I am trying to install on Ubuntu 14.04 LTS 64 bit and am having difficulties.  I have followed various processes e.g. (https://community.nxp.com/docs/DOC-1442 )  without success.  I am going to try one I found for patching LTIB for the IMX.

Would you happen to know of a process for getting LTIB working on my configuration?

0 Kudos
Reply
1,037 Views
alexander_yakov
NXP Employee
NXP Employee

LTIB is quite old software and initially it was designed to run on redhat-type systems.

It is also possible to run LTIB on ealier versions of Ubuntu with just a minor additional packages installed.

But starting from Ubuntu 12.04, LTIB does not work on Ubuntu without special patch.

Please seach this community for "Ubuntu Ltib patch".

For example please look this link

https://community.nxp.com/docs/DOC-93454

Sorry, MPC8548E-CDS BSP is quite old (more than 10 years old), and we offer it "as is".

0 Kudos
Reply
1,039 Views
alexander_yakov
NXP Employee
NXP Employee

I do not see where "MPC8360E26_20081112-LTIB.iso" is mentioned in AN3094.pdf, I assume this is a typo, because MPC8360 BSP is not applicable to MPC8548E CDS board.

For MPC8548E CDS board please download BSP from this page:

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------