What is the maximum current the GPIO pins can output?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the maximum current the GPIO pins can output?

1,006 次查看
sreeharicp
Contributor I
0 项奖励
回复
1 回复

892 次查看
alexander_yakov
NXP Employee
NXP Employee

There is no limitation for maximum output current in our documentation.You can even short circuit output pin, in this case output current will be limited by internal output resistance of output driver, which is typically 40 ohm (depends on pin)

However, we do not guarantee output voltage, if current is higher than specified value. These values are specified as 6 mA in our documentation. Please see MPC8309 Hardware Specifications, Table 47.
https://www.nxp.com/docs/en/data-sheet/MPC8309EC.pdf

For actual driving capabilities of each processor pin please refer to V-A curves in device IBIS model.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复