What is default state of HID2 in MPC8270?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is default state of HID2 in MPC8270?

ソリューションへジャンプ
1,313件の閲覧回数
sai_jagannathan
Contributor II

We are migrating from MPC8260 to MPC8270. In the datasheet we see the HID2 register but unable to find the default value of the register. We would like to know what is the status of the 4 additional cache registers in MPC8270. (We have initialized only the first 4 cache lines that is available in MPC8260). Are the 4 additional cache lines enabled by default in MPC8270?

タグ(1)
0 件の賞賛
返信
1 解決策
1,233件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

The default value (HID2 = 0000_0000) you can find in the G2 Core Reference Manual (Table 5-11. Settings Caused by Hard Reset).

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,234件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

The default value (HID2 = 0000_0000) you can find in the G2 Core Reference Manual (Table 5-11. Settings Caused by Hard Reset).

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,234件の閲覧回数
sai_jagannathan
Contributor II

Thank you

0 件の賞賛
返信