What is default state of HID2 in MPC8270?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is default state of HID2 in MPC8270?

Jump to solution
1,314 Views
sai_jagannathan
Contributor II

We are migrating from MPC8260 to MPC8270. In the datasheet we see the HID2 register but unable to find the default value of the register. We would like to know what is the status of the 4 additional cache registers in MPC8270. (We have initialized only the first 4 cache lines that is available in MPC8260). Are the 4 additional cache lines enabled by default in MPC8270?

Tags (1)
0 Kudos
Reply
1 Solution
1,234 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

The default value (HID2 = 0000_0000) you can find in the G2 Core Reference Manual (Table 5-11. Settings Caused by Hard Reset).

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,235 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

The default value (HID2 = 0000_0000) you can find in the G2 Core Reference Manual (Table 5-11. Settings Caused by Hard Reset).

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,235 Views
sai_jagannathan
Contributor II

Thank you

0 Kudos
Reply