We are looking a Single Board computer Processor with features of 4 port PCIe x4, two Gbit ethernet port and two Rs-422 port for our product development. Please suggest if any NXP processor which supports these features

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

We are looking a Single Board computer Processor with features of 4 port PCIe x4, two Gbit ethernet port and two Rs-422 port for our product development. Please suggest if any NXP processor which supports these features

1,133 Views
kamalakannanr
Contributor I

We are looking a Single Board computer Processor with features of 4 port PCIe x4, two Gbit ethernet port and two Rs-422 port for our product development. Please suggest if any NXP processor which supports these features

0 Kudos
Reply
1 Reply

994 Views
alexander_yakov
NXP Employee
NXP Employee

Attached our Networking Product Selector guide.

Please look devices:

T1040/T1042 - "Value-performance" segment

T2080/T2081 - mid-performance segment

T4240 - High-performance segment

0 Kudos
Reply