UCC UART not working in normal mode, working fine in loopback

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UCC UART not working in normal mode, working fine in loopback

1,848 次查看
jayanthkumarmj
Contributor I

Hello,

     I am working with mpc8360, I m using UCC as USART and UART, uart is working in loopback mode(GUMR_L[DIAG] = 0x01).

     if I made normal mode i.e(GUMR_L[DIAG] = 0x00). then I will not get the status in transmitter buffer i.e Ready bit in buffer will always high(1);

     same code if I made loopback its working.

     kindly give some guidance.

thank you

0 项奖励
回复
2 回复数

1,441 次查看
alexander_yakov
NXP Employee
NXP Employee

Please check if you have CTS input either permamently asserted, or configired as GPIO (in this case CTS will be permanently asserted internally).

Please look QE Reference Manual, Section 6.5.1 for more details.

0 项奖励
回复

1,441 次查看
pareshchaudhary
Contributor I

Hi ,

I am trying  to run UCC UART on MPC8309 evm. I facing problem in receive data. I can successfully Transmit data from evm but i can't receive data into evm.

Could you please guide me where i need to change for receive ?

0 项奖励
回复